메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Data Reading Addresses: DFL Type04 EEPROMEL Pack01 EEPROMEL Pack02

Latest Updated:12/12/2014

Question:

Is it possible to read data from other addresses in data flash memory while using one of the following libraries to erase or program the data flash memory of an RL78-family product?

  • Data Flash Library Type04
  • EEPROM Emulation Library Pack01
  • EEPROM Emulation Library Pack02

Answer:

Data flash memory cannot be read while operations of the flash library on the data flash memory are in progress.
Suitable Products
Data Flash Libraries
  • 이 기사가 도움이 되셨나요?