메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Does the SH/Tiny Series support the AUD (Advanced User Debugger)?

Latest Updated:06/28/2011

Question:

Does the SH/Tiny Series(SH7124/SH7125) support the AUD(Advanced User Debugger)?

Answer:

The SH/Tiny Series(SH7124/SH7125) does not include the AUD function on the chip.
The followings are recommended to AUD debug on the SH/Tiny Series(SH7124/SH7125).

1. Using the E10A-USB(SH0005KCU02H with AUD function) and MCU board.
For information on the debug MCU board, refer to “Debug MCU Board for SuperH Family”.
http://kr.renesas.com/products/tools/emulation_debugging/onchip_debuggers/e10ausb/child_folder/e10a_usb_options.jsp

2. Using the E200F Emulator and the Eva Chip Unit.
For information on the E200F Emulator, refer to the page E200F.
http://kr.renesas.com/products/tools/emulation_debugging/incircuit_emulators/e200f/e200f_tools_product_landing.jsp
Suitable Products
SH7124, SH7125