메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Error message

Latest Updated:12/01/2011

Question:

*** ERROR F108 Overlapped memory area 'ROM' and 'rom' *** ERROR F108 Overlapped memory area 'RAM' and 'ram'

Answer:

These indicate that the link directive file specification is incorrect.
This error means the areas already defined as ROM, RAM are redefined with different names, rom, ram.
To redefine areas specified as ROM, RAM, use the same name (including uppercase and lowercase).
Suitable Products
  • 이 기사가 도움이 되셨나요?