메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to change MCU in PDG2

Last Updated:08/02/2017

Question:

I want to change an MCU in PDG2 in the same manner as CS+ and e² studio. How can I do that?

Answer:

PDG2 does not support MCU changing. To change MCU part number (including ROM/RAM size change), a project needs to be newly created.
Suitable Products
e² studio
CS+ (formerly CubeSuite+)
Code Generator
  • 이 기사가 도움이 되셨나요?