메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to check the code of Peripheral Driver Generator V.2 generate?

Latest Updated:01/29/2015

Question:

How can I check the source code of the library (the Renesas Peripheral Driver Generator Library) called by the functions that the Peripheral Driver Generator V.2 generates?

Answer:

The source files of the Renesas Peripheral Driver Library are stored in the "source/RX" folder in the folder where the Peripheral Driver Generator is installed.

Example of the path: C:\Renesas\PDG2\source\RX

Suitable Products
Peripheral Driver Generator
Renesas Peripheral Driver Library