메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to deal with this error message "Illegal ROM Data file name"?

Latest Updated:09/15/2006

Question:

I am getting the error message "Illegal ROM Data file name". How should I deal with it?

Answer:

There are two possible reasons for this message.
1.There is a space in the path of the hexadecimal data file Spaces cannot be used in directory names or file names. (Example: "My Documents", "Program Files", etc.)
2. The mask file was made with only OSD font data which was set for the hexadecimal file.
When setting only OSD font data, make the hexadecimal data file so that FFh is set at more than 1 byte in the ROM area, then set it as a program file. Refer to Appendix A in the MM User's Manual for details on file formats.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering
  • 이 기사가 도움이 되셨나요?