메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to deal with this error message "Illegal file format"?

Latest Updated:09/15/2006

Question:

I am getting the error message "Illegal file format". How should I deal with it?

Answer:

This error message is displayed in the following cases:
1. When making a mask file
The content of the hexadecimal data file is not a form that MM can work with.
2. When displaying mask information from a mask file
There is an error in the mask file contents (the mask file is damaged).
3. When extracting hexadecimal data from a mask file
There is an error in the mask file contents (the mask file is damaged).

If you receive this error message, refer to Appendices A and B of MM User's Manual for instructions on how to confirm the contents of the file.

Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering
  • 이 기사가 도움이 되셨나요?