메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to fill in ROM Programming Confirmation, Mark Specification Form?

Latest Updated:09/15/2006

Question:

How should the following forms be filled out? (1) ROM Programming Confirmation Form, Mark Specifications Form

Answer:

Please refer to the following examples.
(1) ROM Programming Confirmation Form
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering