메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How to install the emulator bugger that connects through USB port?

Latest Updated:09/22/2003

Question:

After installing the emulator debugger and connecting the emulator through the USB port, the new device is still not recognized by the system.

Answer:

Use the Windows Device Manager to confirm whether your PC is recognizing the USB driver. Select one of the following and right-click on Properties.

Renesas Emulator -> Renesas USB Interface
Mitsubishi Emulator -> Mitsubishi USB Interface
Mitsubishi Emulator -> Renesas USB Interface
Does the [Device Status] display indicate [This device is working properly]?

If the device cannot be found, use the following procedure to install the USB device driver.

  1. Confirm that the emulator debugger has been installed.
  2. Connect the host machine and the emulator with the USB cable.
  3. Turn the emulator power on.
  4. When the USB device is detected, the installation wizard for the corresponding device driver will start up.
  5. By following the messages displayed by the wizard to execute the install process, a dialog will open for specifying the setup information file (inf file).
  6. Specify the musbdrv.inf file under the directory that installed the emulator debugger.
The emulator that contains the USB interface cannot use the USB device driver that comes standard with the OS. You will need to install the driver that comes with the emulator debugger (musbdrv.sys).
Suitable Products
M38000T2-CPE
M34509T2-CPE
M34559T2-CPE
M34571T2-CPE
M30620T-CPE
M34552T2-CPE
M34519T2-CPE
M34514T2-CPE
PC7501
PC4701U
PC4700H
PC4700L
PC4701HS
PC4701L
PC4701M