메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is it necessary to regenerate the Mask file?

Latest Updated:09/15/2006

Question:

[M16C, 7900, 7770, 38000, 740/7450/7470, 7600, 7200, 4500, 720, OSD, ASSP] The Maskfile converter (MM) has been upgraded after my Maskfile has been generated. Is it necessary that I should regenerate the Maskfile?

Answer:

For details concerning the contents of MM upgrades, please refer to " here". And, if you need to regenerate the Maskfile, please contact your Renesas sales office right away.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering