What happen to section: L1120 address not assigned to section name
Latest Updated:09/10/2007
Question:
I got an error message "L1120(W) Section address is not assigned to section name".
What happens to the appropriate section ?
What happens to the appropriate section ?
Answer:
The appropriate section is assigned to right after the section with the biggest address of all the sections that are assigned to the optimizing linkage editor.
Suitable Products
C/C++ Compiler Package for SuperH Family |
C/C++ Compiler Package for H8SX, H8S, H8 Family |