메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why can't I input data for setting the mask using Create Mask File?

Latest Updated:09/15/2006

Question:

I am using MM V.3.00 Release 1 and I have specified the part name and use of the data for setting the mask available area in the MCU information registration. But I cannot input the data for setting the mask available area using the Create Mask File wizard.

Answer:

V.3.00 Release 2 or later versions now have no restrictions on this function.
Please download the newest version.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering
  • 이 기사가 도움이 되셨나요?