메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why error existed when I fix my program with MM Create Mask File Wizard?

Latest Updated:09/15/2006

Question:

I get an error when I specify my program file (hexadecimal file) with the MM Create Mask File Wizard. What's the problem?

Answer:

Make sure there isn't a space, tab or kanji character in the program file name or in the name of the directory in which the program file is located. This type of code in a program file name or directory name will cause an error.
Please remove this code from a program file name or directory name.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering
  • 이 기사가 도움이 되셨나요?