메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why there's an error when I use MM to process an Intel HEX file?

Latest Updated:09/15/2006

Question:

When I use MM to process an Intel HEX file that was created with a partner cross tool, I get an error.

Answer:

An unrelated record was probably included in the Intel HEX file created with a partner cross tool when the mask data was created. When using MM, please use the type of Intel HEX file that can be processed by MM or use a Motorola S format file.
For more details on what type of files can be processed by MM, please refer to "Appendix A: Hexadecimal Data File Formats that MM Inputs" in the MM Users Manual.
Suitable Products
Maskfile Converter
4500 Series ROM Ordering
720 Series ROM Ordering
38000 Series ROM Ordering
740/7450/7470 Series ROM Ordering
7600 Series ROM Ordering
7200 Series ROM Ordering
7770 Series ROM Ordering
M16C Family ROM Ordering
R8C Family ROM Programmed Shipment Ordering
QzROM Programmed Shipment Ordering
ASSP ROM Ordering
OSD Controller ROM Ordering
  • 이 기사가 도움이 되셨나요?