메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Stack frames saved w/ setjmp() return by longjmp() when using CA850?

Latest Updated:12/01/2011

Question:

How do the stack frames saved with setjmp() return by longjmp() when using the CA850?

Answer:

Stack frames are not used with setjmp()/longjmp().
With these functions, global variables are used for data exchange.
Suitable Products
 
  • 이 기사가 도움이 되셨나요?