메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Where to find the available setting on IO Wizard?

Latest Updated:09/04/2009

Question:

After I have set the port direction to output, I would like to do port level setting. But I could not find available setting on IO Wizard.

Answer:

IO Wizard only support port direction selection for initialization setting. After the output source files are generated, user can manually add in the port level setting line in the main function or after port direction setting line in init function.
Suitable Products
  • 이 기사가 도움이 되셨나요?