메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why IO Wizard didn't support timer calculation?

Latest Updated:09/04/2009

Question:

For timer peripheral settings, the IO Wizard did not support timer calculation when external clock is selected as count source frequency for timer mode operation. Why ?

Answer:

In order to run the timer calculation, a known timer count source frequency value is required. Calculation cannot be carried out for external clock because it is an unknown frequency to IO Wizard engine.
Suitable Products
  • 이 기사가 도움이 되셨나요?