메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Why is the following error message is output?

Latest Updated:12/01/2011

Question:

Why is the following error message is output?

Answer:

This error message is output when the branch enabled range (22 bits) of the jarl instruction used for function call in the CA850 is exceeded.
Specify the -Xfar_jump option.
For details, refer to 5.4 "Far jump Call from C Language Program" in the CA850 C Language User's Manual.
Suitable Products
 
  • 이 기사가 도움이 되셨나요?