메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Are there limitation in using Ethernet and the camera on the DK-S7G2 kit?

Latest Updated:10/17/2016

Question:

Are there limitation in using the camera and Ethernet on the DK-S7G2?

Answer:

Yes, there are limitations. Specifically, the Ethernet 1 port shares pins with the camera, so they can't be both used at the same time. The Ethernet 0 port can be used with the camera however.
Suitable Products
DK-S7G2
  • 이 기사가 도움이 되셨나요?