메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Can I run multiple GDB Instances within e2 studio?

Latest Updated:01/14/2017

Question:

Can I run multiple instances of the debugger, GDB, within e2 studio?

Answer:

Yes you can. The below description document shows how.

Multiple GDB Instances while using E2Studio.pdf

Suitable Products
e2 studio
SSP
  • 이 기사가 도움이 되셨나요?