메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How do I get I-Jet working with my Synergy Kit?

Latest Updated:07/11/2016

Question:

How do I get I-Jet working with SSP and my Synergy Kit?

Answer:

The attached preliminary I-Jet Settings Guide is a fairly comprehensive guide to the IAR I-Jet debugger. It includes a guide to connecting I-Jet to your kit, configuring the debugger and what to do in the most common situations when things are not working as you expect (a simple to follow check list).
 
I-Jet
  • 이 기사가 도움이 되셨나요?