메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How do I Create a Synergy Custom Board Support Package?

Last Updated: 11/20/2015

Question:

How do I create a custom Board Support Package (BSP) for a Synergy project?

Answer:

You can easily create a custom BSP by following the guidelines shown in this application note.

 

  • 이 기사가 도움이 되셨나요?