How do I manually integrate the GCC toolchain into e2 Studio and SSP?
Latest Updated:06/21/2016
Question:
How do I manually integrate the GNU ARM Compiler toolchain in my e2 studio and SSP installation?
Answer:
You can manually integrate the GNU ARM toolchain manually by following the below steps:
1) Within e2 studio Preferences (available via Window> Preferences), select C/C++ / Renesas / Renesas Toolchain Management and then manually point e2 studio to the location of the GNU ARM Toolchain (as shown in the screen capture below:

2) Click Add and you get an Add New Toolchain window (as seen below):

3) Put in the location of the Toolchain Path and click OK. The toolchain will be added and should then be integrated into e2 studio.