메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How do I assign a const that resides in Flash not SRAM?

Latest Updated:10/18/2016

Question:

How do I assign a const to Flash memory instead of SRAM? I have a big table and I don't want it to use up SRAM.

Answer:

You can simply put the keyword "const" before the variable and it will be assigned to Flash memory. 

const char s;

Suitable Products
SSP
  • 이 기사가 도움이 되셨나요?