메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How do I change the granularity on the ThreadX tick clock?

Latest Updated:09/19/2016

Question:

The default granularity on the ThreadX clock Tick is 10ms. Is there a way to change this?

Answer:

The granularity of the Tick on ThreadX will be changeable via a CGC API call in a future SSP release. When the release date is available this post will be updated with that information. Once the API is available an example use will be show here.

 

  • 이 기사가 도움이 되셨나요?