메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

How do I invoke custom_bsp_creator correctly?

Latest Updated:10/18/2016

Question:

How do I invoke custom_bsp_creator correctly? Can you show me a working example?

Answer:

Here is an example you can modify as needed for your own BSP. 

custom_bsp_creator.exe -p "C:\Renesas\e2_studio_5_0_0_042\internal\projectgen\arm\Packs\Renesas.Synergy.1.1.0.pack" -b s7g2_dk -# R7FS7G27H2A01CBD -n customs7g2 -d output --verbose

And here is an example for custom_pack_creator:

custom_pack_creator.exe -p output -n customs7g2  -v 1.1.0 -t -e C:\Renesas\e2_studio_5_0_0_042 --verbose

Starting with SSP 1.2.0-b1 the Custom BSP Creator will be built into the ISDE.

Suitable Products
SSP