메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

IBIS Models for Synergy MCUs

Latest Updated:10/04/2016

Question:

Where can I get IBIS files for Synergy MCUs?

Answer:

IBIS models for Synergy S7G2 MCUs are available now for both 3.0 and 3.3V systems. These files are attached to this article below. You can also find IBIS models in the Downloads Tab on the Synergy MCU web page. Foe example- this is the location for the IBIS models for the S7G2.

https://www.renesas.com/en-us/produc...7-series.html#

Note that you can select IBIS/BSDL to search for these file types.

  • 이 기사가 도움이 되셨나요?