메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is there a project export command in IAR EW for Renesas Synergy?

Latest Updated:10/04/2016

Question:

Is the a project export command in IAR EW for Renesas Synergy?

Answer:

There is unfortunately no export feature available yet in the IAR EW for Synergy. You need to backup the SRC folder (customized files), configuration.xml,  pincfg and the .EWW, .EWP and .EWD IAR project files. You SHOULD NOT backup the Synergy/SSP folder- it shouldn't be distributed this way due to the Synergy License agreement- and it will be regenerated by the Generate Project Content button anyway.

Once the project is loaded in the new machine (Project->Open Workspace -> .EWW) or environment you only need to "Generate Project Content".

Suitable Products
IAR EW for Renesas Synergy
  • 이 기사가 도움이 되셨나요?