메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

R_SCI_UART Module Guide References

Last Updated:02/24/2017

Question:

Where can I find the references to module guide resources for the UART HAL module on r_sci_uart?

Answer:

The UART module guide is targeted for SSP 1.2.0 and the SK-S7G2 Kit.

The UART module guide describes what the UART HAL module does, how to add it to your project, how to configure it, the associated APIs and provides an application project with a code walk through so you can quickly learn how to use the UART HAL module in your own design. We recommend that you have the SSP ISDE open and inspect the module stack, configuration information and code while reading over the application project description.

 

Additional resources available to learn more about the SSP UART HAL module are listed below:

 

Know issues for the SSP UART HAL module are listed below:

  • No known issues as of posting date
UART on r_sci_uart module (SSP 1.2.0)

  • 이 기사가 도움이 되셨나요?