메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

SSP Version 1.4.0 Usage Notes

Last Updated:03/30/2018

SSP Version 1.4.0 usage notes can be found in the attached PDF.

The usage notes include issues and workarounds for BSP, HAL, Framework, and Express Logic modules, as well as MCU implementation/SW architecture.

sspv140-v101_Additional-Usage-Notes.pdf

 

  • 이 기사가 도움이 되셨나요?