메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Test of How To Article

"Last Updated" copy

Overview

Explains how to build a Synergy application on command line, without using the ISDE (E2Studio) as a build environment. This is especially important for archiving a certain application release, as for specific version and release management policies that might be used in development.

Goal

After completing this how-to you will be able to store your synergy project in any local folder, and reproduce the build process offline.For this you will not need E2studio installed on the PC used for the build.

Prerequisites

test test test test test test

Setup

test test test test test test

What's Next

test test test test test test
  • 이 기사가 도움이 되셨나요?