메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What can I do with Synergy kits?

Latest Updated:10/11/2016

Question:

Synergy Kits are a great way to quickly come up to speed on the capabilities of the Synergy Platform. 

Answer:

Synergy Kits provide a hardware platform on which you can learn, hands-on, about Synergy Devices, Synergy software tools and the entire Synergy Platform.

A Starter Kit is a perfect way to begin using the Synergy Platform. You can quickly take an example design through the entire Synergy tool flow including creating a project, writing code, compiling, downloading and debugging. Once you have an LED flashing on your board, you are ready to dive into doing your own design.

With a Development Kit you can begin creating your own design using the wide variety of board-supported peripherals and the associated software API's available within e2 studio and the Synergy Software Package (SSP). These boards are also easily expandable using industry standard interfaces to make it easy to include additional capabilities for prototyping and proof of concept exercises.

A Product Example is a complete design and includes a wealth of documentation so you can quickly customize the design to create a real product.

Capabilities and Limitations

To get a more detailed view of the capabilities and limitations of the various kits, and to find out what you can do with the Kits you can view a video that helps you determine the best kit for your needs. You can view this video on the Renesas Presents YouTube channel:

Kits Video is here: https://www.youtube.com/watch?v=1kMf0DniKrA&index=5&list=PLgUXqPkOStPu_uZCwn_1tM2QZIRDhcbCR 

Synergy Playlist Here: https://www.youtube.com/playlist?list=PLgUXqPkOStPu_uZCwn_1tM2QZIRDhcbCR 

Next Steps

To purchase a Synergy kit visit your favorite distributor web site and search their inventory for Renesas Synergy Kits.