메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What are the specifications for the DK-S3A7 V2 LCD Panel?

Latest Updated:10/11/2016

Question:

What are the specifications for the LCD Panel for the DK-S3A7 V 2.0?

Answer:

The specifications are attached in the below documents.

DK- LCD Specification is here:

DK-S3A7-LCD_v2.0.pdf

The Data Sheet is here:

LXD-M7190A_DS_(4.3_300NIT_RT).pdf

FEMA Specification is here:

Fema_T6022A-1PRPO_BEV_B_.pdf-revHEAD.svn000.tmp.pdf

A sample design is attached here:

new_slcdc_test2.zip

 

Additional code and documentation is here:

S3_slcdc.zip

DK-S3LCDv2.0.docx