메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the current SSP revision and when is the next release scheduled?

Latest Updated:5/14/2018

Question:

What is the current SSP revision and when is the next scheduled release?

Answer:

The current revision of SSP is 1.4.0 and the next release, 1.5.0, is currently scheduled for Sept 2018.
Suitable Products
SSP
  • 이 기사가 도움이 되셨나요?