메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What support does SSP offer for bootloading?

Latest Updated:10/24/2016

Question:

What support does SSP provide for bootloading?

Answer:

In the current SSP release, 1.1.3 there is no support for a traditional user bootloader function- i.e. a function that helps load code into flash that is targeted for start-up execution. There are plans for such a function in a future SSP release however. When a public schedule is available, that date will be posted to this artcle.

Note that a user bootloader is different from the Renesas Flash Programmer- or RFP- tool. This tool allows programming of the factor installed boot 'segment', something not done very often. You can find out more about the RFP tool here: 

https://www.renesas.com/en-us/doc/pr...ej0100-rfp.pdf 

Suitable Products
SSP
  • 이 기사가 도움이 되셨나요?