메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Where do I find updates to the DK-S7G2 kit documentation and examples?

Latest Updated:10/13/2016

Question:

Where do I find updates to the DK-S7G2 kit documentation, examples and issues?

Answer:

You can find updates to kit information, example designs and any important issues that might impact your design productivity here.

1) What are the right switch settings to enable JTAG on the board so I can communicate to it for programming and debugging?

What are the JTAG switch settings for Synergy kits to enable debugging?

  • 이 기사가 도움이 되셨나요?