메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Where to get a Synergy Software Package license file?

Latest Updated:10/13/2016

Question:

I've downloaded and installed e2studio ISDE and Synergy Software Package. When creating a new project, I'm asked to point to the valid license file. Where do I find it?

Answer:

ISDE requires valid license file in order to decrypt and compile selected SSP components. After installing Synergy Software Package, the license file is found in the e2studio_install_directory\internal\projectgen\arm\Licenses\ directory. The license file needs to be selected only once. It will then be used as the default for every new project, with an option to select another one, should you or your company choose to acquire developer or production license for the Synergy Software Package.

 

  • 이 기사가 도움이 되셨나요?