메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

r_acmphs Module Guide Resources

Last Updated:02/27/2018

Question:

Where can I find the references to module guide resources for the High Speed Analog Comparator HAL module on r_acmphs?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The ACMPHS HAL module implements the Comparator API for signal processing applications on r_acmphs. It supports the ACMPHS peripheral available on the Synergy microcontroller hardware. A callback is available to signal the user application on transition events.

This module supports the following features:

  • Callback on rising edge, falling edge, or both
  • Configurable debounce filter
  • Option to include comparator output on VCOUT pin

 

Module Guide

The High Speed Analog Comparator module guide is not yet available.

 

Module Guide Resources

There are currently no resources available for the High Speed Analog Comparator.

 

Known issues

  • Refer to the most current SSP release notes for any known issues.
Suitable Products
SSP
  • 이 기사가 도움이 되셨나요?