메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

r_sce_trng Module Guide Resources

Last Updated:11/27/2017

Question:

Where can I find the module guide resources for the TRNG HAL module on r_sce_trng?

Answer:

The TRNG HAL module doesn't have its own module guide. It is included in the r_sce module guide. The resources article for the r_sce module is available here.
SSP
  • 이 기사가 도움이 되셨나요?