메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

r_sdmmc Module Guide Resources

Last Updated:11/21/2017

Question:

Where can I find the module guide resources for the SDMMC HAL module on r_sdmmc?

Answer:

The SDMMC HAL module doesn't have its own module guide. It is included in the Express Logic FileX framework module guide. The resources article for the sf_el_fx module is available here.
SSP
  • 이 기사가 도움이 되셨나요?