메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

r_ssi Module Guide Resources

Last Updated:5/29/2018

Question:

Where can I find the references to the module guide resources for the r_ssi HAL module?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The I2S HAL module is a high-level API for the generic I2S audio serial communication protocol and it is used to send or receive uncompressed audio data in master mode.

The I2S HAL module used with the SSI peripheral in I2S master mode supports the following features in addition to the standard I2S protocol:

  • Full-duplex I2S communication (SSI channel 0 only)
  • Interrupt driven data transmission and reception
  • Integration with the DTC transfer module.
  • A user-defined callback can be created to respond to the need for additional data.

Module Guide

The I2S HAL module guide has been removed from the Renesas web site. It will be replaced sometime in the future. This article will be updated once it has been replaced.

Module Guide Resources

  • Content provided as it becomes available.

Known issues

  • Refer to the most recent release notes for known issues, available here.
Suitable Products
SSP
  • 이 기사가 도움이 되셨나요?