메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

sf_thread_monitor Module Guide Resources

Last Updated:02/28/2018

Question:

Where can I find the references to module guide resources for the Thread Monitor Framework module on sf_thread_monitor?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The Thread Monitor Framework provides high-level APIs for thread monitor framework applications and configures the watchdog timer (WDT) or independent watchdog timer (IWDT). The Thread Monitor Framework uses WDT or IWDT peripherals on the Synergy MCU device.

The Thread Monitor Framework supports the following features:

  • The Thread Monitor Framework interface monitors RTOS threads using a watchdog timer. The Thread Monitor forces a watchdog reset of the microcontroller when any of the monitored threads do not behave as expected.
  • The Thread Monitor is designed to support any Synergy device with either a WDT or IWDT peripheral, and a HAL module with no changes to the API.
  • In profiling mode, the minimum and maximum counter values for registered threads can be determined. When in profiling mode, the watchdog timer is always refreshed and does not reset the device.
  • Both the WDT and IWDT HAL modules are supported by this framework module.

Module Guide

The Thread Monitor Framework module guide is targeted for SSP 1.2.0 and the SK-S7G2 Kit.

The most recent versions of the Thread Monitor Framework module guide application note, application project and import guide are available here

Module Guide Resources

The Thread Monitor Framework module is used in the Services Developer Examples available for the SK-S7G2. You can find a Knowledge Base article that describes the Developer Examples and how to use them here.

Known issues

  • Refer to the most recent release notes for known issues, available here.
Suitable Products
SSP
  • 이 기사가 도움이 되셨나요?