메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

tx_src Module Guide Resources

Last Updated:03/01/2018

Question:

Where can I find the module guide resources for the ThreadX Source module on tx_src?

Answer:

Information on the module guide itself and the associated resources and known issues are available here.

Introduction

The ThreadX Source Module provides configurable options for a wide range of ThreadX properties. These include properties for:

  • Timer settings
  • Stack settings
  • Priority settings

 

Module Guide

The ThreadX Source module guide is targeted for SSP 1.2.0 and above.

The ThreadX Source module guide is available here.

Module Guide Resources

The following useful user manuals are included in the X-Ware documentation package available here.

  • ThreadX User’s Manual

 

Known issues

  • Refer to the SSP release notes for known issues, available here.

 

Suitable Products
SSP
  • 이 기사가 도움이 되셨나요?