메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

What is the current SSP revision and when is the next release scheduled?

Latest Updated:10/18/2017

Question:

What is the current SSP revision and when is the next scheduled release?

Answer:

The current revision of SSP is 1.3.0 and the next release, the 1.3.1 release is scheduled for Q4 of 2017.
Suitable Products
SSP