메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

IP Address of TPS-1 Set and Retrieved by Host MCU

Last Updated:06/01/2017

Question:

Can you get and set the IP address of TPS-1 by the host MCU?

Answer:

Yes, the driver software includes the APIs to both get and set the IP address.  Please refer to the APIs TPS_GetIPConfig and SetIPConfig in the TPS-1 toolkit driver manual.
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?