메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

Is the bit count be an integral multiple of the 10-bits sign pair length?

Latest Updated:08/01/2005

Question:

For the uPD98408 ATM PHY, is the interval (bit count) between adjacent pairs of signs separated by the IDLE pattern in the PHY output direction so as to be an integral multiple of the sign pair length (10 bits)?

Answer:

Yes, that is correct.
Suitable Products
BD/DVD Recorder
Digital Camcorder
Industrial Network
  • 이 기사가 도움이 되셨나요?