메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

TPS-1 API Compiler Independence

Last Updated:06/02/2017

Question:

Is the API independent of the C Code Compiler? For example, for Cortex-M3 GNU tools?

Answer:

The API code was created to use ANSI C code to make the API as compiler independent as possible.
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?