메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

TPS-1 Firmware Updates via Host MCU

Last Updated:06/01/2017

Question:

Can the TPS-1 firmware be updated by a host MCU?

Answer:

Yes, the software driver includes the APIs to do this.  Please refer to “Firmware Update Over Host Interface” in the TPS-1 toolkit driver manual.
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?