메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

TPS-1 Monitoring and Diagnostics for SFP Fiber via I2C

Last Updated:06/01/2017

Question:

Can the TPS-1 provide and monitor diagnostics for SFP fiber optic communication via I2C?

Answer:

Yes, this can easily be set in the TPS-1 configurator.
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?