메인 콘텐츠로 건너뛰기
Knowledgebase
Home
Renesas Korea

TPS-1 PROFINET Stack and Updated GSDML Files

Last Updated:06/01/2017

Question:

Does the GSDML file change as the TPS is updated?

Answer:

Every version of the TPS-1 development toolkit comes with a set of GSDML files that reflect the feature set implemented in the current PROFINET stack. These files comply with the requirements of the current PROFINET and GSDML specifications.
Suitable Products
TPS-1
  • 이 기사가 도움이 되셨나요?